Title

Kokeile etsiä avainsanoilla, tuote- tai tilauskoodilla tai sarjanumerolla, esim. "CM442" tai "tekniset tiedot"
Aloita haku syöttämällä vähintään 2 merkkiä.

Endress+Hauser fully acquires startup

PCR-based molecular analyses complement Endress+Hauser’s portfolio for process and laboratory applications

Julkaisupäivä 05.11.2026

Endress+Hauser BioSense becomes a fully integrated part of the Endress+Hauser Group

PCR-based technology complements the portfolio for process and laboratory applications

Full integration lays the foundation for the startup’s further development

Endress+Hauser acquired the remaining shares in Endress+Hauser BioSense from Hahn-Schickard gGmbH on 1 November 2026. As a result, the company has become a wholly owned subsidiary of the Endress+Hauser Group. Endress+Hauser BioSense develops PCR-based detection systems for rapid molecular analysis directly on site.

Technology expands process analytics

With this acquisition, Endress+Hauser is strengthening its portfolio for analytical and quality measurements. Endress+Hauser BioSense technology complements traditional process analysis techniques and enables rapid PCR analyses without the need for a fully equipped laboratory or specially trained personnel. In the beverage industry, for example, this technology allows beer to be tested for specific microorganisms directly on site to detect potential contamination at an early stage. Other applications in the food & beverage, water quality and life sciences sectors, as well as in data centers, cover industries and fields in which Endress+Hauser is already active.

“Solutions of Endress+Hauser BioSense bring molecular analysis closer to the process and open up additional opportunities for our customers to monitor quality and hygiene. With this full acquisition, we aim to further develop the technology in a targeted manner and integrate it even more closely with our existing portfolio for process and laboratory applications,” says Dr Mirko Lehmann, Chief Technology Officer at Endress+Hauser.

Successful collaboration as the foundation for further development

Endress+Hauser BioSense was founded in 2021 as a joint venture between Endress+Hauser and Hahn-Schickard in Freiburg im Breisgau, Germany, and today employs 15 people. The goal of the partnership was to adapt technologies from molecular diagnostics for use in industrial process and laboratory automation. Endress+Hauser previously held a 75 percent stake, while Hahn-Schickard held 25 percent.

Hahn-Schickard contributed its expertise in microfluidic technology to the collaboration. Together, the two companies developed a solution for industrial process and laboratory automation. With the acquisition of the remaining shares, Endress+Hauser will now continue to develop PCR-based analysis systems of Endress+Hauser BioSense under its sole responsibility.

“Endress+Hauser BioSense is the result of a close and trusting collaboration. Together, we have succeeded in combining our expertise in microfluidics and molecular diagnostics with Endress+Hauser’s experience in industrial applications. We are pleased that the jointly developed technology will now be continued and further developed under the Endress+Hauser umbrella,” says Professor Roland Zengerle, director of the Hahn-Schickard Institute.

Lue samanlaisia aiheita

Lataukset

Tutustu lisämateriaaleihin

document icon
EH_2026-11-05_BioSense.zip ZIP, 5 MB
download icon Lataa

Lehdistölista

Pysy ajan tasalla ja liity Endress+Hauserin lehdistölistalle.
Endress+Hauserin lehdistölista

Endress+Hauser lähettää säännöllisesti lehdistötiedotteita ajankohtaisista aiheista ja yrityksen tiedoista viestinnän ammattilaisille.

Valitse sinua kiinnostava aihe:  *
Valitse sinua kiinnostavat alat: *
Henkilötiedot

*-merkityt kentät ovat pakollisia. Saat sähköpostiin tilausvahvistuksen. Tietojen antaminen on vapaaehtoista ja tietoja käytetään ainoastaan uutiskirjeiden personointiin, eikä niitä luovuteta kolmansille osapuolille. Tilastollisista syistä suoritamme linkkien seurannan anonyymisti.

Yhteydenotto

Lisätietoja saat asiantuntijoiltamme

Martin Raab Head of Public Communication and Group Media Spokesman, global
Kägenstrasse 24153 Reinach BL Sveitsi
pictogram email Lähetä sähköposti
Puh. (ensisijainen) +41 61 715 7722
Faksi +41 61 715 2888