Kokeile etsiä avainsanoilla, tuote- tai tilauskoodilla tai sarjanumerolla, esim. "CM442" tai "tekniset tiedot"
Aloita haku syöttämällä vähintään 2 merkkiä.

TECOSOL achieves stable biodiesel production with robust instrumentation

Reliable measurement technology stabilizes processes under variable operating conditions

Teollisuudenala: Kemia
Biodiesel production process: stable operation with integrated measurement technology
Pyydä lisätietoja tarjonnastamme

Täytä alla oleva lomake lisätietojen pyytämistä varten.

Kerro meille mahdollisimman yksityiskohtaisesti, kuinka voimme auttaa sinua. Näin voimme antaa sinulle mahdollisimman tarkan vastauksen.

Yhteenveto

TECOSOL is one of the leading biofuels manufacturers in Europe. They operate 2 plants and produce biofuel that achieves significant CO₂ savings compared to fossil diesel. Highly contaminated residues and waste materials, fluctuating feedstock compositions, high temperatures and vacuum conditions place demanding requirements on biodiesel production processes and instrumentation. Using the complete product portfolio from Endress+Hauser, TECOSOL GmbH operates a highly automated plant in Wittenberge that ensures cost-efficient, safe and stable production.

Ralf Türck, managing director of Tecosol

“With biodiesel from the new plant in Wittenberge, TECOSOL achieves over 90% CO₂ savings compared to fossil diesel. It represents one of the few effective solutions for decarbonization."

Ralf Türck, Managing Director, TECOSOL GmbH

The challenge: biodiesel production under feedstock variability and demanding process conditions

TECOSOL GmbH produces biodiesel from contaminated residues and waste materials generated, for example, in the timber industry and oleochemistry. The composition of these feedstocks varies significantly, requiring sophisticated process engineering. Safe control of high-temperature and high-pressure processes is required for the production of high-quality biofuel.

Storage and loading also present significant challenges. The tank farm must accurately record all inventories and correctly reflect storage and handling processes. It also needs to ensure transparent custody transfer subject to legal metrology for all material flows. The company’s goal was to realize a highly automated plant for continuous product and process monitoring even under variable raw material flows and complex process conditions.

Our solution: engineered instrumentation for reliable biodiesel production

From planning through to commissioning, TECOSOL GmbH, Endress+Hauser and the appointed project engineer worked in close partnership. Through intensive exchange and close coordination, the instrumentation was designed to meet the specific requirements of varying residues and waste materials, withstand high temperatures, pressures and vacuum conditions and be seamlessly integrated into the automation system.

Whether level, point level, flow, pressure or temperature, the complete product portfolio from Endress+Hauser covers all applications at the plant in Wittenberge, including analytical measurement technology and automation components.

Yhteydenotto

Oletko kiinnostunut tarjonnastamme? Haluaisitko keskustella ratkaisuista sovelluksiisi?

Pyydä lisätietoja tarjonnastamme

Täytä alla oleva lomake lisätietojen pyytämistä varten.

Kerro meille mahdollisimman yksityiskohtaisesti, kuinka voimme auttaa sinua. Näin voimme antaa sinulle mahdollisimman tarkan vastauksen.

Products and services used

/

Related solutions and technology

Lämpötilamittaus

Prosessiteollisuuden lämpötilamittarit ja lähettimet

Lisätietoja

Ohjelmistoratkaisut

Asiaankuuluvien mittaus- ja järjestelmätekniikoiden lisäksi tarjoamme kaikille teollisuudenaloille sopivia ohjelmistotyökaluja, jotka pitävät huolen prosessien täydestä toimivuudesta..

Lisätietoja

Painemittaus

Paine- ja paine-eromittaukset nesteille, kaasuille ja höyryille

Lisätietoja

Pintamittaus

Jatkuva pintamittaus ja pintakytkin mittaus nesteille ja kiintoaineille

Lisätietoja

FAQs

Yrityslogo: S-IU - PSR - Template

TECOSOL GmbH on yksi Euroopan johtavista biopolttoaineiden tuottajista. Yrityksen pääkonttori on Ochsenfurtissa, ja se valmistaa polttoaineita, jotka säästävät merkittävästi hiilidioksidia. TECOSOL on rakentanut Wittenbergenin laitokselleen uuden biodieseltehtaan, joka on varustettu kokonaan Endress+Hauserin mittausteknologialla. Laitos asettaa uudet standardit kestävälle tuotannolle ja kiertotaloudelle.